Other Parts Discussed in Thread: OMAP-L137, DP83640,
Using the evaluation board "OMAP-L137", we achieved an ethernet sustainable rate of 30 Mbps, far from the theoretical maximum of 100 Mbps. Can it be due to limitations of the DSP or the driver? or can it be due to the peripherals of the evaluation board?
In our final design, we plan to use the TMS320C6745 with the ethernet transceiver DP83640, including IEEE1588 clock synchronization. Anyone have recommendations or documentation about it?