I want to access PMU of A72 on TDA4VM for QNX + RTOS,mode.
Now build success, but run failed:Illegal instruction.
I should access PMU as kernel not user.
How should I create the kernel and how to access the PMU?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to access PMU of A72 on TDA4VM for QNX + RTOS,mode.
Now build success, but run failed:Illegal instruction.
I should access PMU as kernel not user.
How should I create the kernel and how to access the PMU?
Hi Guoxun,
When using QNX the concept of "kernel mode" vs " user mode" is not present. Please reference the below link for an overview of this - Microkernel architecture (qnx.com). Additional resources for QNX are available from that link.
Regarding the "illegal instruction", this indicates the QNX process which is running has hit an exception. Typically this would be due to a memory access to a module that is not clocked or powered, or possibly to an access to a memory address that the running S/W does not have the correct privilege to access.
The ThreadCtl() API can be referred to for increasing / decreasing IO privilege, if the failing access is due to IO privilege.
Regards,
kb
Hi kb,
Is there an example about get access to PMU for QNX? A whole process include power on and ThreadCtl()?
PMU as a coprocessor, does it need special processing?
For "When using QNX the concept of "kernel mode" vs " user mode" is not present."
Is it means that there is no need to create a kernel for "kernel mode" in QNX system and there is no "kernel mode" for QNX system?
Thanks,
Guoxun
Hi Guoxun,
TI SDK for QNX does not include any A72 PMU based example code. Some generic links on PMU are below.
The csl_*Pmu*() functions in TI SDK for RTOS file, ti-processor-sdk-rtos-j721e-evm-07_02_00_06/pdk_jacinto_07_01_05_14/packages/ti/csl/arch/a53/src/csl_a53.c, can be referenced as a starting point.
Regards,
kb
Hi kb,
Is PMU of A72 power on by default?
Now I access to the PMU with instruction msr/mrs(like csl_a53.c): build success, but run failed( Illegal instruction).
The value that get from PMUSERENR_EL0 with the instruction mrs is 0, and the instruction msr run failed.
Why?
Is the PMU power off by default? How to power on it ?
Hi Guoxun,
In testing on PSDK QNX 7.1, the csl_a53.c, xxCycleCounter APIs when ported to a QNX executable, functioned as expected. No additional steps were required in terms of clocking and power settings from A72.
For permission to access the PMU registers had to add the below.
if (ThreadCtl(_NTO_TCTL_IO_PRIV, NULL) == -1) {
perror("ThreadCtl(_NTO_TCTL_IO_PRIV");
}
Regards,
kb
Hi kb,
Now I can get the cycle count with PMU, but the value is much bigger than expected. Code is as below:

and the result is as below:

Only one add instruction takes 60 cycle counts.(and the cycle counts is different for each execution sometimes.)
Another questions:
When get the value as in the example in csl_a53.c:

the result is as below:

the value of val (the return value of function getPMUCycleCount()) is different from the value of cycleCount (the get value of function getPMUCycleCount() in main()). Why?
If get the value as below, the value of val is the same as the value of cycleCount :

What's the reason?
Regards,
Guoxun
Hi Guoxun,
Regarding the number of cycles for the test case, there is an API in csl_a53.c, CSL_getPmuCycleCountOverhead() which will show the overhead of starting/stopping the counter. This overhead would be need to be taken into account, as well as the assembly code generated for the test.
Regards,
kb
Hi kb,
I get the overhead about starting/stoping the counter, it's about 60 cycle counts, is this normal?
the value of val (the return value of function getPMUCycleCount()) is different from the value of cycleCount (the get value of function getPMUCycleCount() in main()).
What may cause this question?
Result show:"val is 63", but I get the value with function getPMUCycleCount() is 10(result shows "cycle count is 10").
Regards,
Guoxun