Part Number: TDA4VM
HI
i used two chip tda4 make a custom board, two tda4 communicate using sgmii,pinseeting is SERDES1 SGMII4 the gpio is AG15 AF16 AJ15 AH16
my base sdk is RTOS-07-03-00-07 QNX-07-03-00 LINUX-07-03-00-05
i found e2e had a same problem
and i check the source code i think if changed the pinmux the function maybe ok
What changes should I make to enable mac to mac communicat with SGMII4
best Regards