This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA76P: using 488d0000.usb as usb gadget for adb (SDK v6AO.1.1)

Part Number: DRA76P
Other Parts Discussed in Thread: J6EVM5777

Hi,

I have the j6evm5777 using android  SDK v6AO.1.1 all the SW and the HW is by default.

To connect via adb, the usb configured is the usb 48890000.usb.

I want to use the usb 488d0000.usb but if I can't. I checked /sys/class/udc and I can only see 48890000.usb

In the "USB Composite Gadget Using CONFIG-FS on DRA7xx Devices" doc the example is with the 48890000.usb.

Is it possible to configure the 488d0000.usb as gadget to use adb over it.

Best regards,

Miguel