Other Parts Discussed in Thread: PMP, CCSTUDIO
Dear all,
Details of Hardware
Processor : Dm8168
SATA Device:TOSHIBA IH3671 chip (ADVANTEC 32G MSATA Industrial Solid State Drive, 820 MLC 4-Channel (-40~85C))
In Our customized board SATA1 and SATA2 is not working(Detection is failing after multiple software reset). Please find the below error log .
ISSUE: Always the ata link status is down, Sata is not working and link speed is 1.5Gbps
-----------------------Error Log related to SATA-------------------
ata1: softreset failed (device not ready)
ata1: softreset failed (device not ready)
ata1: link is slow to respond, please be patient (ready=0)
ata1: softreset failed (device not ready)
ata1: limiting SATA link speed to 1.5 Gbps
ata1: softreset failed (device not ready)
ata1: reset failed, giving up
ata2: SATA link down (SStatus 0 SControl 300)
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
----------------------------------End----------------------------------------------------------------
The following links i studied
http://patchwork.ozlabs.org/patch/73713/
http://arago-project.org/git/projects/?p=linux-omap3.git;a=commitdiff;h=84a34fba9ad4cc00736ad577893f87a3d0f10e19;hp=18b1f21d313ba77d037a746bab193982ead4e905
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/287768/1004424.aspx
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/150493.aspx
But If the same Kernel Image and SATA device tried in the EVM_dm8168 board SATA is working fine and link speed is 3Gbps, please find the below Log
ata1: softreset failed (device not ready)
ata1: applying PMP SRST workaround and retrying
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1.00: ATA-8: SQF-SMSM4-32G-S8E, S8FM06A7, max UDMA/133
ata1.00: 62533296 sectors, multi 16: LBA48 NCQ (depth 31/32)
ata1.00: configured for UDMA/133
scsi 0:0:0:0: Direct-Access ATA SQF-SMSM4-32G-S8 S8FM PQ: 0 ANSI: 5
sd 0:0:0:0: Attached scsi generic sg0 type 0
sd 0:0:0:0: [sda] 62533296 512-byte logical blocks: (32.0 GB/29.8 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
sda: sda1
sd 0:0:0:0: [sda] Attached SCSI disk
ata2: SATA link down (SStatus 0 SControl 300)
EXT3-fs: barriers not enabled
kjournald starting. Commit interval 5 seconds
EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended
EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: mounted
What may be the Issue ??
Please let us know your suggestions on the above mentioned queries
Any input from the forum members would be highly appreciated.
Thanks
Narthan S