Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hi experts.
I am developing DSP RTOS program on IDKAM5728.
I configured a timer interruption. Days ago, I found that it don't interrupt strictly per 2ms when I set it as a 2ms interruption.
So I wrote some code to test it (I have changed the period as 10 ms ).
#include <xdc/std.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/timers/dmtimer/Timer.h>
//#include <ti/sysbios/hal/Timer.h>
#include "c6x.h"
void timerIsr2ms(UArg arg);
Void taskFxn(UArg a0, UArg a1);
Timer_Handle timerHandle;
/*
* ======== main ========
*/
Int main()
{
Task_Handle task;
Error_Block eb;
System_printf("enter main()\n");
Error_init(&eb);
task = Task_create(taskFxn, NULL, &eb);
if (task == NULL) {
System_printf("Task_create() failed!\n");
BIOS_exit(0);
}
Timer_Params timerParams;
Timer_Params_init(&timerParams);
timerParams.period = 10000;
timerParams.runMode = Timer_RunMode_CONTINUOUS;
timerParams.periodType = Timer_PeriodType_MICROSECS;
timerParams.arg = 0;
timerParams.extFreq.lo = 1000000;
timerParams.extFreq.hi = 0;
timerParams.startMode = Timer_StartMode_USER;
timerHandle = Timer_create(Timer_ANY, timerIsr2ms, &timerParams, &eb);
if (timerHandle == NULL)
{
System_abort("Timer create failed");
}
BIOS_start(); /* does not return */
return(0);
}
Void taskFxn(UArg a0, UArg a1)
{
Timer_start(timerHandle);
int delay;
while(1)
{
Task_sleep(10);
System_flush();
};
}
unsigned int start=1, finish=1,time=0;
void timerIsr2ms(UArg arg)
{
finish = TSCL;
time = (finish-start);
start = TSCL;
System_printf("timer time is %d\n",time);
}
and there is my cfg file:
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Error = xdc.useModule('xdc.runtime.Error');
var Log = xdc.useModule('xdc.runtime.Log');
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Main = xdc.useModule('xdc.runtime.Main');
var Memory = xdc.useModule('xdc.runtime.Memory')
var SysMin = xdc.useModule('xdc.runtime.SysMin');
var System = xdc.useModule('xdc.runtime.System');
var Text = xdc.useModule('xdc.runtime.Text');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
//var Timer = xdc.useModule('ti.sysbios.hal.Timer');
//Timer.intFreq.lo = 20000000;
//Timer.intFreq.hi = 0;
/*
* Minimize exit handler array in System. The System module includes
* an array of functions that are registered with System_atexit() to be
* called by System_exit().
*/
System.maxAtexitHandlers = 4;
/*
* The BIOS module will create the default heap for the system.
* Specify the size of this default heap.
*/
BIOS.heapSize = 0x1000;
/*
* Build a custom SYS/BIOS library from sources.
*/
BIOS.libType = BIOS.LibType_Custom;
/* System stack size (used by ISRs and Swis) */
Program.stack = 0x2000;
/* Circular buffer size for System_printf() */
SysMin.bufSize = 0x200;
/*
* Create and install logger for the whole system
*/
var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.numEntries = 16;
var logger0 = LoggerBuf.create(loggerBufParams);
Defaults.common$.logger = logger0;
Main.common$.diags_INFO = Diags.ALWAYS_ON;
System.SupportProxy = SysMin;
there is some of its output:
some time is strange.
And I have tried to configure intfreq as 20M and not to configure extfreq.
It get the similar outcome or even a worse one.
any help will be appreciated.
Regards
Yx