Part Number: PROCESSOR-SDK-AM65X
Tool/software: TI-RTOS
Hi,
do you have any feedback why building 5.2 version takes much longer than 5.1? This is for build all.
Do you experience the same?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PROCESSOR-SDK-AM65X
Tool/software: TI-RTOS
Hi,
do you have any feedback why building 5.2 version takes much longer than 5.1? This is for build all.
Do you experience the same?
Thorsten,
Can you please indicate your host build environment. Are you building in Windows or Linux. Our observation from nightly builds using Yocto infrastructure shows all components in PRSDK 5.01 and PRSDK 5.02 took comparable amount of time with slightly higher time for the latest SDK.
Having said that, as an application developer, users should not have to gmake clean and build the entire SDK. There are several libraries like CSL, driver libraries, OSAL that most customers would not need to rebuild unless there is a bug/patch they want to apply to those components.
Additionally, there are some flags that will help reduce build times significantly.
Here are my notes from Processor SDK RTOS build and testing that might be useful to you to build some of the components and reduce build times:
The key is to do targeted builds for the platform you are working on, for the core you are working on. Hope this helps,
Regards,
Rahul
PS: Also, there is an effort to enable parallel make in the that you can track using bug ID PRSDK-4574 and PRSDK-5247. This should help reduce the build times.
I am reposting the notes in the document so it is searchable for other community users. These notes will be added to Software developers guide soon.
PRSDK PDK build notes:
The following steps can be used in a command shell to generate the CCS projects for PDK low level drivers. Users are expected to complete component discovery in CCS before using these steps.
Setup environment from root directory:
<SDK_INSTALL_PATH>\processor_sdk_rtos_am65xx_x_xx_xx_xx
setupenv.bat
Optional step: SDK contains prebuilt binaries for driver and CSL libraries so there is no need to rebuild the libraries but if you need to rebuild the libraries, you can do it using gmake utility using the following options.
gmake <target>_clean
gmake <target>
<target>: Refer to makefile in the pdk_am65xx_x_x_x\packages
all csl board emac fvid2 gpio i2c mcasp mmcsd nimu pm profiling pruss sciclient spi uart udma usb sbl sa osal can be used as <target>
This can take a while to build. To limit the build to A53 core, use the additional arguments as
gmake <target> LIMIT_BOARDS=am65xx_evm LIMIT_CORES=mpu1_0 <ARGUMENTS>
|
ARGUMENTS |
Options |
Description |
|
LIMIT_BOARDS |
am65xx_evm, am65xx_idk |
Supported evaluation platform |
|
LIMIT_SOC |
am65xx |
Supported SOC options |
|
LIMIT_CORES |
mcu1_0, mpu1_0 |
Support for different cores |
|
DISABLE_RECURSE_DEPS |
yes, no |
Disable for building dependencies |
|
BUILD_PROFILE |
release, debug |
Build profile |
Caution: With DISABLE_RECURSE_DEPS=yes, you will run into link time errors if dependent component libraries are not built.
To apply the options globally, set the environment variables and then invoke the build
set LIMIT_BOARDS=am65xx_evm
set LIMIT_SOC=am65xx
set DISABLE_RECURSE_DEPS=yes (Use only if dependent components are already built)
set BUILD_PROFILE=release (Default setting is release)
Regards,
Rahul