Part Number: PROCESSOR-SDK-DRA8X-TDA4X
Other Parts Discussed in Thread: DRA829, TDA4VM
Hardware Setup:
- CCS
- Spectrum Degital XDS560V2 STM USB Emulator
- EVM J721E_DRA829_TDA4VM
- PDK having GEL file to flash
- Enable ECC in GEL file
- SET DDRSS_ECC_CTRL_REG bit[0] and bit[1]. which should be before loading data into LPDDR4
- Specify start and end address range in DDRSS_ECC_R0_STR_ADDR_REG and DDRSS_ECC_R0_END_ADDR_REG. In those register only bit{18:0] are usable and [31:19] are reserved. Now LPDDR4 start address is 0x80000000. How to write this start address in the [18:0] bits? Same question for end address.
- How to set interrupt for SEC and DEC and how to route it into MCU domain?
- Do i need to configure anything else?
- Initialize LPDDR4 (already there in GEL file)
- Load firmware
- Enable ECC check in boot process DDRSS_ECC_CTRL_REG bit[2]
Any help appreciated