Other Parts Discussed in Thread: LMX2572LP
Is there any documentation available to assist selecting decoupling capacitors for use with the AFE7071?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you for your reply.
The schematic you linked to is from the AFE707x development PCB. On the development PCB, there are typically 3 decoupling capacitors per power supply pin. This is more decoupling capacitors on the power supply pins than I expected to see. For example, the LMX2572LP is the IC recommended to generate the LO signal for the AFE7071. The data sheet for the LMX2572LP recommends 1 capacitor per power supply pin. Why, then, does the AFE7071 need so many more?
JMT82,
Sorry, but I did not work on this board. After looking at the schematic in more detail, I would suggest the following:
Only use one 0.1uF cap for each DVDD, CLKVDD, DACVDD, IOVDD, MODVDD, and FUSEVDD pin. Try to place these as close as possible to the pin.
Use at least one bulk 10uF and 1uF cap for each regulator output along with an EMI filter such as a Murata NFM31PC276B0J3.
Regards,
Jim