Other Parts Discussed in Thread: ADS62P49, TRF371109, TRF371125, , TRF3710
The datasheet is mostly silent on the VCM pin, except when it is contradictory. The pin definition is "Baseband common-mode input voltage", implying it is an input, but then in "ELECTRICAL CHARACTERISTIC" it has: Vcm | Output, common-mode | Measured at I- and Q-channel baseband outputs | 1.5 V
So, is it an input or an output? If it is an input (as shown in the EVM documentation), what is the range of voltages over which it is compliant?