Team,
What does the “Min Full scale input power, at device pins” on page 22 refer to?
Does it refer to the power at 100 ohms, i.e. approx. 0.9Vpp?
As a full-scale value, I would have expected a voltage value.
Is only the power important in this case, so would using a 1:1 balun not yield any other full-scale performance?
Which data does the NFMin of approx. 22dB specified in the data sheet refer to?
I can't fully understand the calculated value.
Best regards