This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX8410LEVM: LMX8410LEVM: Can't possible to read the value of registers over USBtoANY

Part Number: LMX8410LEVM
Other Parts Discussed in Thread: USB2ANY

Tool/software:

Dear,

I try to work with LMX8410LEVM eval board. And I use USBtoANY tool. The problem is that I have try to readback any of registers I have received 0x0000. I checked the SPI data and clk is ok. And I see the data at readback procedure is ok, but the TICS sofware say 0x0000 anyway. When I wroye all the registers eval board led is on and I think it os work correctly. Can't check, but I can see the reaction. So, could you advice how I can readback the registers correctly? After programming all the registers to default configuration from TICS menu it start correctly the LED has switched on. Then I wrote R0[2] to 0. So, to enable reading on MUXout(MISO) channel. Anyway I see the correct data on the oscilloscope during readback operation (everything like in datasheet), but the TICS software said the data is still 0x0000 in any of register.