Hi,
I would like to buy a TRF37D73 EVM to amplify a signal with a frequency of 73 MHz and another signal that ranges from 50 MHz to 800 MHz. It says on the page that the TRF37D73 EVM has a 20dB gain for a 2.5GHz frequency, the TRF37x73 and TRF37x75 EVM User’s Guide doesn't specify the gain for the range from 1MHz to 6GHz where the TRF37D73 is functional. Is there any way to know the gain at a specific point (for instance: 73MHz)?, I would like to know if at this frequency the EVM still has a gain and if it is posible to tune the EVM, is it?.
Regards,
Angel