This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF89: no output data / single tone

Part Number: DAC38RF89
Other Parts Discussed in Thread: LMK04816

Hello!

I have a custom DAC38RF89 board with no JTAG available.

Here is my use conditions:

- dacclk=328MHz, PLL, interpolation=24

- single DAC, LMFS=22210, K=16

- JESD204b subclass 0 (sysref internally genereted)

For now, I have progress with JESD204b passing most of SerDes tests (PRBS-7/23/31) and link tests (k28.5, d21.5) according to lane alarms and sync status stable HIGH.

But when running in "non-test flow" there is no output data from DAC, I mean no data at all - no matter configured as normal operation or constant single tone (0x12F 0x0001 / 0x130 0x7FFF).

My config with actual reg data is in attachment.

Thanks!

Alex

dac38rf89.cfg)