art Number: DAC38RF89
The cofiguration of DAC38RF89 is follow. I use DUC1 as I data path, and DUC2 as Q data path. I enable the MIXERAB and the NCOAB of the two path, and add adjacent DAC path AB sample(Q data) to I data,then output the sum.
But at the output, the power of signal is loss 12dB. When I set MIXERAB_GAIN=1,the power is loss 6dB.
Why are the power losses 12dB and 6dB respectively in the two case?