OK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Xiao,
The easiest way to see if the DAC PLL is working is to check the loop filter voltage value, which is page 0, address 0x6, bits 7:5. If the PLL is working properly, these three bits should report a decimal value between 3 and 5. If the PLL is not locked, this value will be either 0 or 7 decimal.
Another check is to place the part in NCO only mode. If the NCO output is at the proper frequency, the DAC PLL is operating properly.
If you have access to the CLKTX output, this also will tell you if the PLL is operating properly or not.
Make sure miscellaneous register 0x3B (page 4) has bit 15 set to "1". This bit determines if the DAC is to use the PLL or an external clock.
Regards,
Jim
Hi, Jim:
The miscellaneous register 0x3B (page 4) has bit 15 indeed is set to "1".
The miscellaneous register 0x31 (page 4) has bit 10 indeed is set to "1".
The miscellaneous register 0x0C (page 4) has bit 0 indeed is set to "0" (There are no reference about it ,I don't know exact meaning aobut it).
Also there is a file attached in the post, can you check it and give extra help ?
Thanks
Are you tuning the VCO? This must be done to get the PLL to lock. The GUI does this function when you click on PLL Auto Tune.
I made a mistake. I need you to read back register 0x05. From what I am seeing from register 0x06, the VCO is not locked.
Hi,Jim:
register 0x05 page 0 = 0x0139 (before I read register 0x5@page 0, I clear all fields of register 0x5 to make sure that it is not a sticked value)
Yes , I tried to tune the VCO. But I will double check the tuning sequences right now.
Best Regards
Xiao,
Your assumption regarding the temp sense read back is correct. 29d = 29 C.
Your PLL is not locked since bit 0 of add 0x5 = 1. Are you providing a 512MHz reference clock to the DAC? Is this single-ended or differential? What is the amplitude? Make sure the values in page 4 of address 0x31 are set properly.
Regards,
Jim
I provide reference clock to the DAC .It is a differential LVPECL clock from LMK05318. The differential amplitude is above 800mV. Register 0x31 @ page 4 is set 0x0400.
512M_ref_pll_821.cfgXiao,
I have my PLL locked on my EVM using your settings with an external 512MHz diff clock. The config file is attached. Give this a try.
Regards,
Jim