Hi everyone,
I ‘am working with the PGA460 device. I ’am using the demo board hardware with a custom software. I have also installed a custom board for the transformer and the ultrasonic transducer. With this transformer I reach 250V peak-peak driving voltage for the transducer. Everything went well until I lost all my signals on the PGA460 reading. After an investigation I find out that the resistor on the INP pin was dead (R41). I think that the resistor could not withstand the higher voltage. What do you think about that?
This problem raises another question. I ‘am planning to raise my voltage up to 1000V. What is the maximum voltage that the PGA460 is able to support on his INP pin? (On the datasheet the value is 2V, I think that is very low). What kinds of protection are implemented in the PGA460 for the INP and INN pin which are directly exposed to the high driving voltage of the transducer?
Thank you.