Hi, I need some help because I am a little lost. I developed a driver to control the OP3101 EVM board. The driver was working fine but now, I have designed a custom board with the OPT3101. The board is very simple and it shall work fine but here is the problem:
When I try to write some parameter via I2C, I am able to see on the oscilloscope the I2C frame with all the parameters (address, data and ACK) but then when i try to read the written value over the register always read the default value.
Somebody knows why is it happen? Some issue related with this topic?
Thanks in advance.