Hi Team,
There is a good news that we have a chance to replace "NCP3335AMN330R2G"
Do we have a solution to replace "NCP3335AMN330R2G" ?
The URL below is "NCP3335AMN330R2G" datasheet
https://www.onsemi.com/pdf/datasheet/ncp3335a-d.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
There is a good news that we have a chance to replace "NCP3335AMN330R2G"
Do we have a solution to replace "NCP3335AMN330R2G" ?
The URL below is "NCP3335AMN330R2G" datasheet
https://www.onsemi.com/pdf/datasheet/ncp3335a-d.pdf
Kygo,
No p2p options available. Below are the possible solutions.
NCP3335A | TPS7A26 | TLV767 | LP38693-ADJ | LP38691-ADJ | |
AEC Q100 | NO | NO | NO | NO | NO |
Output Options | Adjustable Output, Fixed Output | Adjustable Output, Fixed Output | Adjustable Output, Fixed Output | Adjustable Output | Adjustable Output |
Iout (Max) (A) | 0.5 | 0.5 | 1 | 0.5 | 0.5 |
Vin (Max) (V) | 12 | 18 | 16 | 10 | 10 |
Vin (Min) (V) | 2.6 | 2.4 | 2.5 | 2.7 | 2.7 |
Vout (Max) (V) | 10 | 17.41 | 14.5 | 9 | 9 |
Vout (Min) (V) | 1.25 | 1.24 | 0.8 | 1.25 | 1.25 |
Fixed Output Options (V) | 1.5, 1.8, 2.5, 2.8, 2.85, 3, 3.3, 5, ADJ | 1.25, 1.8, 2.5, 3.3, 5 | 0.8, 1.8, 2.8, 3.3, 5 | - | - |
Enable | YES | YES | YES | YES | NO |
Power Good | NO | YES | NO | NO | NO |
Output Capacitor Type | Ceramic | Ceramic | Ceramic | Ceramic | Ceramic |
PSRR @ 100KHz (dB) | 20 | 22 | 53 | 45 | 45 |
Noise (uVrms) | 58 | 300 | 60 | 80 | 80 |
Accuracy (%) | 1.5 | 1 | 1 | 2 | 4 |
Vdo (Typ) (mV) | 260 | 355 | 900 | 250 | 250 |
Iq (Typ) (mA) | 0.19 | 0.002 | 0.05 | 0.055 | 0.055 |
Thermal Resistance θJA (°C/W) | 66 | 73.3 | 60.1 | 51 | 51 |
Min Package Area (mm2) | 9 | 4 | 4 | 9 | 9 |
Package Type | WSON, MSOP | WSON | HVSSOP, WSON | SOT-223, WSON |
WSON |
Regards,
Prakash L