Other Parts Discussed in Thread: DRV425
Hi Team,
Can you please help us regarding the customer's concern below.
I have been experimenting with the DRV425 and I am consistently getting an output value that is 1.31 times the value calculated per Equation 1. With B=0.5mT, my output value is 1.60 volts. Should be 1.218 based on Rshunt =49.9ohms. My supply voltage is 3.3V. I can't figure out why I have that discrepancy/ Do you have any ideas?
I use these devices in a linear array and they are spaced about 0.6" apart. Would that have any influence? I wouldn't think so, but I thought I would ask.
Regards,
Danilo