This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV421: DRV421 output voltage

Part Number: DRV421

Hello

I'm designing a current sensor using the DRV421that seems to work very well

My question is : if I have only to measure positive currents what is the best way to get a 0/5V signal (0V-->Imin=0Ampere  5-->Imax)?

Should I add and external fast operational amplifier in order to remove the 2.5V offset and get the correct amplification or can I directly work with the internal differential amplifier?

Even a range 0.5V/5V  (0.5-->Imin=0Ampere  5V-->Imax) can be acceptable like other commercil sensor with ratiometric output

Thank you very much

Nicola