Other Parts Discussed in Thread: AWR1443
Hi,
I am setting up AWR1443BOOST with DCA1000 EVM to do some data capturing. Following are the details for the setup
- AWR1443 ES3
- mmWave Studio 2.1.1.0
The document I am following is DCA1000 Quick Start Guide(www.ti.com/.../spruik7.pdf. The following screenshot shows the status after proper connection to the host.
And I am trying to run DataCaptureDemo_xWR.lua to see the behavior of the setup. The original script has some issue working with AWR1443, after some minor modification, it can run till the post processing part. Following log shows the last part of the running log.
The post processing screen shot is as following
It shows an object at 5m position while there is not. Even I turn the setup to face another direction, it still returns the same data. I have checked the timestamp of the data file(.bin), they are update at every new capture, so there should not be data/file residue issue.
Any suggestion to tackle this problem? Thanks in advance.