I figured out that I have to build the code under Linux, but I am having trouble with the process to get it to run. Do I still need a Windows machine that runs mmWave Studio? If so, does the mmWave Studio have to run a Lua script that grabs frames from the sensor?
I've tried it every way that I can figure out, but nothing seems to be working. My latest setup has the DCA1000EVM going into a switch and my Linux computer connected to the same switch. I set the IP{ address of my Linux machine to 192.168.33.30 and then run the Linux CLI program. I run it with the fpga, record, and then record_start options, but nothing seems to ever come across the wire.
Thank you.
Shawn