Other Parts Discussed in Thread: IWR6843ISK-ODS
Hello everyone,
I want to connect a IWR6843ISK-ODS and DCA1000EVM to a Raspberry Pi. When I connect the FTDI of the DCA1000EVM to the Pi via USB, the Pi detects a FTDI Device with the correct product name and serial number but does not load a driver or attach a port. I think this is a driver problem. Because its a Linux System on ARM I cannot use the drivers provided with the SDK and CCS but have to go the FTDI page.I know that there are two possible FTDI drivers: the VCP and D2XX. Could you just verify for me which of these 2 drivers is the correct one in general for the DCA1000EVM FTDI?
Thank you!
Lars