Hi
I have an AWR 1843 and DCA 1000. Using the DCA 1000, I capture the ADC samples. Then using the Matlab script given in the TI document, I have converted this adc_data.bin file to the adc_data.mat file.
In this mat file, I have complex numbers at every position. Now for further processing, I have divided these samples according to my chirp configuration. My questions are:
1. All the complex numbers are received voltages or powers? what is the unit of this (mV or volts) or (mW or W)
2. When I have treated these as voltage (Volts). And doing the FFT and plotting the range plots, the amplitude at Y-axis is 15 dB. How can it be greater than 0 dB? Note: The range of the target is correct; only the amplitude is not correct.
3. What it needs to do for calibrating the amplitude to the correct value?
4. What is the noise floor of this device?