Hello Champs,
With below register settings, PMIC_CLKOUT of 12MHz frequency is working.
* EXTCLKSRCSEL - 0x2 (600MHz PLL)
* EXTCLK2DIV : 0x0 (div1)
* Average of MIN Div and MAX Div : 0x32 (50)
[Q1] (AWR6843) Is it possible to have PMIC_CLKOUT of 24MHz frequency? If it is possible, can you guide how to set the registers?
[Q2] (LP87524) When using the PMIC_CLKOUT as 12MHz, how to set the PMIC (LP87524) switching frequency as 12MHz?
When he changed the PMIC register (EXT_CLK_FREQ) as 0x11 (12MHz), the switching frequency was still 4MHz, not 12MHz. (The PLL_CTRL setting was 0x8B [1000 1011])
Is there something more to do for the switching frequency of PMIC?
Thanks and regards,
Hayden