Hi,
pressed the wrong button, meant to REPLY! One last question on this then I will close the thread - promise!
I suspect the answer may be either that this is too deep to discuss here, or that on the lines of that's what the SDK means by "only s/w trigger supported"...
trying to use h/w trigger, things do happen (as seen in output) but, even though it seems to say everything has completed just as it does for s/w trigger, trying to do another run leads to the response:
Status: Failed, Error Type: API IS ISSUED WHEN FRAMES ARE ONGOING
Is there anything I can send API wise to recover from this, other that a complete hard restart of everything (STOP FRAME doesn't seem to do it)? Or is it that I need to send multiple triggers (per frame?) rather than just once to start things off?
many thanks
Alan