This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Spurious reflections in FFT profile

Part Number: IWR6843ISK
Other Parts Discussed in Thread: DCA1000EVM, MMWAVEICBOOST, IWR1443BOOST

Hello,

I have set up the IWR6843ISK+MMWAVEICBOOST+DCA1000EVM and ran the data capture demo LUA script DataCapturedemo_xWR.lua from the mmWave studio (v. 2.0.0.2). I can gather the I/Q reflections, 2D FFT, and range FFT. However, I see a very strong reflection at the 0th distance of the Radar. This is the default LUA script and the IWR6843ISK device is ES1.0. Attaching the output from the mmWave studio and the hardware picture. As you can see, there is nothing near to the Radar, but still a strong reflection at the 0th distance. Could you please help? Thanks!