Other Parts Discussed in Thread: LMT01,
Hi there,
I want to make sure that the TMP117 is the appropriate solution to our engineering problem. It has an acceptable working range and accuracy. However, in our application we will be measuring the temperatures of several items inside a thermal chamber.
Will long lead lines add measurement error to the system?
Since the TMP117 requires a micro-controller, is there one that is recommended for robust operation?
Will we be able to connect up to 30 sensors on the same 2 wire bus? If so, will that affect the resistors we attach to the system?
It appears that the available packages are designed for board mounting; is there another package that could be used without a board so that it can be in direct contact with the item under test?
Can these ICs interface with LabVIEW software?
If the TMP117 isn't right for our application, can you recommend an IC that might be? Temp range: -50 to 90C. Desired accuracy > 0.25 degC.
Thanks,
J