This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm trying to use DCA1000 with IWR6843ISK-ODS board to do some raw data captures.
I just installed mmWaveStudio and all the dependencies. I had set up the jumpers and carrier mux's as described here: https://e2e.ti.com/support/sensors/f/1023/t/781420?IWR6843-Not-working-with-DCA1000 . I also erased the SFlash memory before connecting the whole setup to the mmWaveStudio. All the Connection steps go well, including loading of the BSS and MSS images. However, it fails when I try to press the "SPI Connect" button.
Here are the log messages from the very beginning and till the point of getting an error. Note, the last two errors happen when I press the "SPI Connect" button. Any tips on that?
GM: Constructor
GM: Fri Oct 01 15:46:34 2021
RSTD.Transmit("/Settings")
[15:46:35]
[15:46:35] ### Running Startup script: "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
[15:46:35] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[15:46:35] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[15:46:35] Scripter ignored: Attempt to UnBuild() again or before Build.
[15:46:35] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[15:46:35] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[15:46:35] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[15:46:35] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[15:46:35] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[15:46:35] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[15:46:35] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
[15:46:35] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[15:46:35] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[15:46:35] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[15:46:35] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[15:46:35] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[15:46:35] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[15:46:35] RSTD.Transmit("/")
[15:46:35] RSTD.SaveSettings(): Settings saved to "C:\Users\kibong\AppData\Roaming\RSTD\config.xml"
[15:46:35] RSTD.Build()
[15:46:35] RSTD.SaveSettings(): Settings saved to "C:\Users\kibong\AppData\Roaming\RSTD\config.xml"
[15:46:35] RSTD.Transmit("/")
[15:46:35] RSTD.AL_Build()
[15:46:35] RSTD.AL_LoadXml()
[15:46:35] RSTD.Transmit("/")
[15:46:35] RSTD.AL_Init()
[15:46:35] RSTD.Clients_Build()
[15:46:35] GM: Init
[15:46:35] GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
[15:46:35] GM: 1 Guest (s) init
[15:46:35] GM: 1 Module(s) init
[15:46:35] GM: 2 Tab (s) init
[15:46:35] RSTD.Client_LoadXml()
[15:46:35] [RadarAPI]: ar1.selectRadarMode(0)
[15:46:35] [RadarAPI]: Status: Passed
[15:46:35] Matlab Runtime Engine is installed
[15:46:35] [RadarAPI]: Starting Matlab Engine..
[15:46:40] [RadarAPI]: Matlab Engine Started!
[15:46:42] [RadarAPI]: ar1.selectCascadeMode(0)
[15:46:42] [RadarAPI]: Status: Passed
[15:46:42] [RadarAPI]: ar1.LoadSettings('C:\Users\kibong\AppData\Roaming\RSTD\ar1gui.ini')
[15:46:42] TESTING = false
[15:46:42] RstdNet: Port 2777: Listening..
[15:46:42]
[15:46:42] ***Script completed successfully.***
[15:48:12] [RadarAPI]: Opening Gpio Control Port()
[15:48:12] [RadarAPI]: Status: Passed
[15:48:12] [RadarAPI]: Opening Board Control Port()
[15:48:12] [RadarAPI]: Status: Passed
[15:48:13] [RadarAPI]: ar1.FullReset()
[15:48:13] [RadarAPI]: Status: Passed
[15:48:14] [RadarAPI]: Closing Board Control Port()
[15:48:14] [RadarAPI]: Status: Passed
[15:48:14] [RadarAPI]: Closing Gpio Control Port()
[15:48:14] [RadarAPI]: Status: Passed
[15:48:14] [RadarAPI]: ar1.SOPControl(2)
[15:48:14] [RadarAPI]: Status: Passed
[15:48:16] [RadarAPI]: ar1.Connect(7,921600,1000)
[15:48:18] [RadarAPI]: Warning: Connected with baudrate 115200
[15:48:19] [RadarAPI]: Warning: Disconnected existing BaudRate
[15:48:19] [RadarAPI]: Warning: Trying to connect with baudrate 921600
[15:48:21] [RadarAPI]: ar1.Calling_IsConnected()
[15:48:22] [RadarAPI]: ar1.SelectChipVersion("IWR6843")
[15:48:22] [RadarAPI]: Status: Passed
[15:48:22] [RadarAPI]: ar1.frequencyBandSelection("60G")
[15:48:22] [RadarAPI]: ar1.SelectChipVersion("IWR6843")
[15:48:22] [RadarAPI]: Status: Passed
[15:48:22] Device Status : IWR6843/QM/SOP:2/ES:2
[15:48:22] [RadarAPI]: ar1.SaveSettings('C:\Users\kibong\AppData\Roaming\RSTD\ar1gui.ini')
[15:48:26] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\masterss\\xwr68xx_masterss.bin")
[15:48:27] [RadarAPI]: Downloading BSS ROM RPRC Binary..
[15:48:30] [RadarAPI]: ar1.GetBSSFwVersion()
[15:48:30] [RadarAPI]: BSSFwVersion:(02.00.00.03 (27/08/19))
[15:48:39] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\radarss\\xwr68xx_radarss.bin")
[15:48:39] [RadarAPI]: Downloading MSS RPRC Binary..
[15:48:46] [RadarAPI]: ar1.GetMSSFwVersion()
[15:48:46] [RadarAPI]: MSSFwVersion:(06.02.01.05 (09/03/20))
[15:48:51] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[15:48:51] Status: Failed, Error Type: RESP TIMEOUT
[15:48:55] MSS Power Up async event was not received!
Hello Kibong,
Glad you were able to solve your problem. Thankyou for providing clarification to the TI E2E community.
Regards,
Ishita