This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Computing Maximum Range, Velocity and Resolution mmWave System

Guru**** 151344 points


This FAQ was written to answer a common request: Computing the Max Range, Range Resolution, Max Velocity, Velocity Resolution for a mmWave Chirp Configuration.

This FAQ provides the theoretical equations and shows how to compute them in an example

  • Maximum Range
  • Range Resolution
  • Maximum unambiguous Velocity
  • Velocity Resolution

Following are the equations to compute these parameters. For more information on the derivation of these equations the reader is invited to review this training

https://training.ti.com/intro-mmwave-sensing-fmcw-radars-module-1-range-estimation?cu=1128486

  • Maximum Range
    • Rmax = (EFs x c)/(2 x S)
      • EFs = Effective Fs = 0.9Fs
      • S: slope of the chirp

  • Range Resolution
    • Rres = c/2B = (EFs x c)/(2*S*ADC_Samples)
      • EFs = Effective Fs = 0.9Fs
      • S: slope of the chirp

  • Maximum Unambiguous Velocity
    • Vmax = Lambda / (4 * ETc)
      • Lambda: Wavelength
      • ETc: Effective Tc = (Idle_Time + rampEndTime) * nb_Tx (for MIMO configuration)
  • Velocity Resolution
    • Vres = Lambda / (2 * Active frame time)
      • Active frame time AFT = Tc * #Tx * #chirps/Tx (for MIMO configuration)

Example for following chirp configuration

profileCfg 1 77 7 3 39 0 0 50 1 128 3600 0 0 36

chirpCfg 2 2 1 0 0 0 0 1
chirpCfg 3 3 1 0 0 0 0 2
chirpCfg 4 4 1 0 0 0 0 4

frameCfg 0 2 128 0 100 1 0

Following are the computed values:

  • Maximum Range
    • Rmax = (0.9*3600e3*3e8 m/s)/(2*50 e12 /s) = 9.72m

  • Range Resolution
    • Rres = Rmax/128 = 0.076m

  • Maximum unambiguous Velocity
    • Lambda (Wavelength) (77Ghz) = (3e8 m/s) / 77e9 /s) = 0.3/77m = 0.003896

    • Tc = Idle_Time + rampEndTime  = (7+39) usec = 46usec

    • Effective chirp time, taking MIMO into account:
      • ETc = 3*Tc = 138usec 
    • Vmax = 3.896e-3m/(4x138e-6)s = 7.05 m/s

  • Velocity Resolution
    • Active frame time AFT = 51x3x128usec = 19584usec = 19.584ms
    • Vres2 = 3.896e-3m/(2x19.584e-3)s = 0.1 m/s