Hello,
I calibrate PGA300 with EVM and GUI.
I have a problem with calibration, so I would like some advice.
Until a while ago, I was able to calibrate without problems.
When I was conducting an accuracy verification test after calibrating a sensor, the OUT voltage value suddenly became unstable.
At the end of the calibration, "successful" was displayed.
Also, when I read EEPROM Variables, there was no problem, but when I restarted the GUI, the EEPROM value changed.
EEPROM value is set to Lock.
The EEPROM value that was changing was 5, and this phenomenon is reproducible.
・Normal pressure lower / upper value
・Clamp value - lower / upper
・Fault configurable value
Since an abnormality has occurred immediately after calibration, I think that the setting at the time of calibration is a problem.
I am in great trouble, so I would appreciate any advice.
Regards,