Dear All,
I am using the AWR1642BOOST EVM. I am trying the driver vital sign lab, but I am experiecing some troubles.
I had followed the indications included in the Getting Started Guide: TI mmWave Lab Driver Vital Signs Version 1.0.0.
After flashing the pre-built binary file:
I removed the jumper form sp02 and I launched the GUI.
No signal is shown, here the messages:
Serial Port Found
Data Port Number is "COM5"
User Port Number is "COM4"
Data port succesfully Open
User port succesfully Open
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
"COM4"
Configuration File Path is %s/n "../../mmwave_automotive_toolbox_3_4_0/labs/incabinsensing/driver_vital_signs/vitalSigns_host/gui/profiles/profile_2d_VitalSigns_20fps_Back.cfg"
"sensorStop"
"flushCfg"
"dfeDataOutputMode 1"
"channelCfg 15 3 0"
"adcCfg 2 1"
"adcbufCfg -1 0 0 1 0"
"profileCfg 0 77 7 6 57 0 0 70 1 100 2000 0 0 40"
"chirpCfg 0 0 0 0 0 0 0 1"
"frameCfg 0 0 2 0 50 1 0"
"lowPower 0 0"
"guiMonitor 0 0 0 0 1"
"vitalSignsCfg 0.1 0.7 256 320 1 0.1 0.05 300000 300000"
"motionDetection 1 20 0.04 0"
"sensorStart"
""
""
"sensorStop"
"flushCfg"
"dfeDataOutputMode 1"
"channelCfg 15 3 0"
"adcCfg 2 1"
"adcbufCfg -1 0 0 1 0"
"profileCfg 0 77 7 6 57 0 0 70 1 100 2000 0 0 40"
"chirpCfg 0 0 0 0 0 0 0 1"
"frameCfg 0 0 2 0 50 1 0"
"lowPower 0 0"
"guiMonitor 0 0 0 0 1"
"vitalSignsCfg 0.1 0.7 256 320 1 0.1 0.05 300000 300000"
0.1
0.7
1
"motionDetection 1 20 0.04 0"
"sensorStart"
""
""
Chirp Duration in us is : 50
Chirp Bandwidth in kHz is : 3500
Maximum Range in Meters is : 4.28571
Range-FFT size is : 128
Range-Bin size is : 0.0334821
Range-Bin Start Index is : 2
Range-Bin End Index is : 20
Total Payload size from the UART is : 220
Padding Factor is : 7
Total Payload size from the UART is : 224
Can someone help me to find out what I am doing wrong?
Thanks in advance,
Elisa