This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a question about static clutter removal.
To remove static clutter, I suppose it has only to ignore zero th doppler data 'after' 2DFFT simply, but SDK subtracts zero th component, which is mean value of the input samples for 2D FFT, 'before' 2DFFT.
Could you let me know the reason why such way is used? Is there any technical reasons?
Hello,
I would appreciate it if you would answer my question.
Please let me know if you need more information concerning this matter.
Hi Kei,
Sorry for the immense delay in my response.
Quite simply, the zeroth FFT bin is the DC component of the signal. If the mean of the signal is subtracted from it before taking the FFT, the DC component and therefore the zeroth FFT bin is zeroed out.
Regards,
Aayush
Hello Aayush,
Thank you for your reply.
I feel you didn’t fully understand what I meant, so please let me try again.
In order to remove static clutter (zeroth doppler objects), why does not SDK do the following procedure?
first: 1D-FFT
next: 2D-FFT
finally: delete zeroth doppler bin data
Regards,
Kei
Hi Kei,
If the DC component isn't subtracted out, bin 0 will have a large value. When windowing, this will leak into the adjacent bins, possibly obscuring weak targets in them. This is why we prefer to remove the DC out altogether than just ignore bin 0.
Regards,
Aayush
Hi, Aayush,
Thank you for your answer.
I understand that clearly.
Regards,
Kei