Hi there,
We are using the IWR1443 radar sensor to do range measurements. We've been experimenting with different parameters for the CFAR configuration and are running into an issue when using a guard window length that is bigger than 7. Any time the guard window length is 7 or lower we are able to take measurements just fine but when we attempt to set this parameter to 8 or higher the sensor's firmware seems to lock up. Are there any constraints to this parameter that we've missed in the documentation? We are using mmWave SDK version 2.1. I've also been able to reproduce this using the mmWave Demo Visualizer 2.1.0 so it seems like it could be an issue with this version of the SDK? The configuration commands are sent and replied to with a "Done" as expected but afterwards no plots can be seen in the Plots tab.
Thank you for the support!