Hello,
I took a stab at deriving X, Y, Z velocity from the radial velocity reported by the chip.
Can you look over my math / trigonometry / equations / vector break down and let me know if my theory is correct?
Thank you
Chris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I took a stab at deriving X, Y, Z velocity from the radial velocity reported by the chip.
Can you look over my math / trigonometry / equations / vector break down and let me know if my theory is correct?
Thank you
Chris
Also just to confirm, positive radial velocity reported from the chip is when the object is moving towards the sensor?
Hi Chris,
The equations look correct to me provided the x, y and z directions are assumed properly.
I think the radial velocity reported by chip is positive as object moves away from radar since phase change will then only be positive. Please refer to slide 37 of this pdf: https://training.ti.com/sites/default/files/docs/mmwaveSensing-FMCW-offlineviewing_0.pdf . Here it clearly shows the phasor moves in anti-clockwise motion (phase is positive) only if object moves away from radar and vice-versa.
Let me know if you have any questions.
Thanks and Regards,
Akshay.
I wanted to ask about a special situation regarding the first drawing on the left where Vxz=Vx cosΘ + Vz cosΘ
if z=0 then Θ = 0 and Vxz = Vx since cos(0)=1 and sin(0)=0 | it doesnt matter what Vz is as it is not measured/reported in the radial velocity
is that correct?
if so then if x=0, Vxz=Vz and if x and z=0 then the object would be at the same position as the sensor and any velocity would not be radial so Vxz=0
is that correct?
Hi Chris,
Give me some time. Let me go through this once more and get back.
Thanks and Regards,
Akshay.
I thought more and wanted to add.
I believe the special case assessment is still correct but to add, if z=0 then Vz can not be determined as it is purely tangential and not measured/reported by the chip.
and if z=x=0, Vz and Vx are purely tangential and neither can be determined.
Hi Chris,
From your diagram analysis you are right. If x=0, z=0, sensor and object are in same position. While if z = 0, Vz is not determined and is purely tangential, so not measured by the chip.
Thanks and Regards,
Akshay.