Other Parts Discussed in Thread: LMP7721
Hello,
I have Some Questions related 4 Electrodes Gas Sensor. Currently, I am working with LMP91000 & LMP7721.
LMP91000 Configuration: ( WE,CE and RE )
VREF DIVIDER = 50%
RTIA = 14K
Rload = 100E
LMP7721 configuration: Auxillary Electrode
VREF DIVIDER = 50%
RTIA = 10K
Rload = 100E
Q-1) As per Josh Wyatt's suggestion, The non- inverting pin of all TIA is Pulled Down. Can I pull down the Vref Pin Externally and what happens if I select positive or negative bias?
Q-2) Whenever LMP7721 is Restart, its Output is Reset. is it necessary for LMP7721 'ON' Continuously (LMP91000 is always ON Condition)?
I use divider at LP7721 with reference to VDD at 50%, same as LMP91000 .( Both Work on 3V3 VDD).
OCV for LMP91000 = 1.65V
OCV for LMP7721 = 1.67V
Q-3) The CO-A4 Sensor took almost 30 min for stabilizing the output. can we reduce this time using CKT?
I am using VDD input in Voltage Divider (50%). The Output voltage is 1.65V ( OCV = Open Circuit Voltage) ( VDD = 3.3V )
Here, I attached some testing ckt conditions, Pease check,s and suggest your best solution.
Thanks
Sagar