As we know, FDC2214 uses parallel resonance to achieve capacitance measurement. And the formula of resonance frequency is f=1/(2pi LC).
I now use single-ended mode,and the sensor is only attached to one end.
In this case, can the sensor and the external capacitance/inductance be considered in parallel?
Or can we use the resonance formula above to calculate the capacitance of the sensor?
In addition, I found this in the documentation SNOA952. Is this the equivalent circuit in single-ended mode?

Best regards!