Tool/software:
Dear Expert
1.What current should be set for the DRIVE_CRENT_CH0 of FDC2214 in order to achieve a sensor oscillation voltage of 1.2-1.8V? Is there a theoretical calculation model for this? What are the issues if the voltage is below 1.2V or above 1.8V?
2. The Reserved bit in the CONFIG register is set to 0 by default, but it is required to be set to 1. What is the reason for this?
3.If InoA &InoB short circurt ,could it cause these IC enter in shutdown mode ?And how to recover to normal state ?