Other Parts Discussed in Thread: IWR6843
1. Is there a way to configure this chipset in CW mode via only 1 of its 3Txs. much appreciated for a config file for such a case using only a single Tx (i.e. w/o mimo)
2. in FMCW I try to configure a chirp with a single Tx and chirp cycle of 4.2uS and receive a lot of errors. would appreciate receiving a config file for a single FMCW Tx (i.e. no MIMO) with chirp to chrip length of 4.2uS covering a RFBW of ~20MHz, other params less important (all the idles around a start sampling time etc.).
much appreciated for the assistance.
Ehud.