Hello,
My case is 0-10V and 0-5 psi differential.
1) If I set up DAC HEX 0/1350/2700 related to 0/2.5/5 psi, calibration does not work, WHY?
2) If I set up DAC HEX 5/1350/2700 related to 0.01/2.5/5 psi, DAC calibration works, and calibrated at 0.01/2.5/5psi, ADC works too.
BUT at 0 psi it is consistent 0.0075 psi off (0.15% accuracy), and at 2.5 and 5 psi accuracy is 0.02% to 0.03%. WHY?
Please advise, thanks in advance.
Ed