We have a custom IWR6843AOP board based off the IWR6843AOPEVM (see attached the relevant sections of the schematic). The PMIC and Flash are the same as the EVM. The Crystal used is different. We are using ABM10W-40.0000MHZ-8-B1U-T3 (https://www.mouser.ca/datasheet/2/3/ABM10W-1774948.pdf), which does fall within the tolerance stated in the IWR6843AOP datasheet.
The NERROR_OUT is being asserted on powerup for both flashing and normal modes. We are currently unable to flash the IWR6843AOP. Any suggestions on isolating the cause of the NERROR_OUT?