This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: DCA1000EVM IWR6843ISK-ODS MMWAVEICBOOST

Part Number: DCA1000EVM
Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843ISK-ODS,

The device we use are DCA1000EVM,IWR6843ISK-ODS and MMWAVEICBOOST, the line connection of the device is shown in the picture.

The DCA1000 SW2 is set up as shown.

And we turned off the firewall, the IP settings are as shown in the picture below.

But we still get errors: 

[09:27:04]  [RadarAPI]: Status: Passed

[09:27:04]  RfInit Success

[09:27:05]  [RadarAPI]: ar1.DataPathConfig(1, 1, 0)

[09:27:05]  [RadarAPI]: Status: Passed

[09:27:05]  DataPathConfig Success

[09:27:05]  [RadarAPI]: ar1.LvdsClkConfig(1, 1)

[09:27:06]  [RadarAPI]: Status: Passed

[09:27:06]  LvdsClkConfig Success

[09:27:06]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)

[09:27:06]  [RadarAPI]: Status: Passed

[09:27:06]  LVDSLaneConfig Success

[09:27:06]  [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0)

[09:27:06]  [RadarAPI]: Status: Passed

[09:27:06]  Test Source Configuration Success

[09:27:06]  [RadarAPI]: ar1.ProfileConfig(0, 60.25, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 131072, 30)

[09:27:06]  [RadarAPI]: Status: Passed

[09:27:06]  ProfileConfig Success

[09:27:06]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0)

[09:27:06]  [RadarAPI]: Status: Passed

[09:27:06]  ChirpConfig Success

[09:27:06]  [RadarAPI]: ar1.EnableTestSource(1)

[09:27:06]  [RadarAPI]: Status: Passed

[09:27:06]  Enabling Test Source Success

[09:27:06]  Test Source Already Enabled...!!!

[09:27:06]  [RadarAPI]: ar1.EnableTestSource(1)

[09:27:06]  [RadarAPI]: Status: Passed

[09:27:06]  [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1)

[09:27:10]  Status: Failed, Error Type: RESP TIMEOUT

[09:27:10]  [RadarAPI]: MatlabProc Status: Failed

[09:27:10]  FrameConfig failure

[09:27:10]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")

[09:27:10]  [RadarAPI]: Status: Passed

[09:27:10]  SelectCaptureDevice Success

[09:27:10]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098)

[09:27:10]  [RadarAPI]: Sending fpga command to DCA1000

[09:27:10]  [RadarAPI]:

[09:27:10]  Invalid lvdsMode value (0). [error -4016]

[09:27:10]  [RadarAPI]: Sending fpga_version command to DCA1000

[09:27:20]  [RadarAPI]:

[09:27:20] 

[09:27:20]  Unable to read FPGA Version. [error -5]

[09:27:20] 

[09:27:20]  CaptureCardConfig_EthInit Success

[09:27:20]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)

[09:27:20]  [RadarAPI]: Sending fpga command to DCA1000

[09:27:30]  [RadarAPI]:

[09:27:30]  FPGA Configuration :

[09:27:30]  Timeout Error! System disconnected

[09:27:30]  CaptureCardConfig_Mode Success

[09:27:30]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)

[09:27:30]  [RadarAPI]: Sending fpga command to DCA1000

[09:27:41]  [RadarAPI]:

[09:27:41]  FPGA Configuration :

[09:27:41]  Timeout Error! System disconnected

[09:27:41]  [RadarAPI]: Sending record command to DCA1000

[09:27:51]  [RadarAPI]:

[09:27:51]  Configure Record :

[09:27:51]  Timeout Error! System disconnected

[09:27:51]  CaptureCardConfig_PacketDelay failure

[09:27:51]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)

[09:27:51]  [RadarAPI]: Sending start_record command to DCA1000

[09:27:51]  [RadarAPI]: Status: Passed

[09:27:52]  [RadarAPI]: ar1.StartFrame()

[09:27:56]  Status: Failed, Error Type: RESP TIMEOUT

[09:28:01]  Please wait for a few seconds for matlab post processing .....!!!!

[09:28:01]  [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")

[09:28:01]  [RadarAPI]: No of files Captured: 1, Total no of frames for each device : 8

So we want to reprogram the FPGA. After the configuration is completed according to the manual, the device information cannot be obtained through jtag after using the diamond programmer to connect the device. After manually selecting the device, the following error is displayed:

Lattice VM Drivers detected (HW-DLN-3C (Parallel), HW-USBN-2B (FTDI))

INFO - Scanning USB2 Port FTUSB-0...

Programmer device database loaded

ERROR - Failed to scan board.

ERROR - Scan Failed - Creating Blank Programmer Project.

INFO - Check configuration setup: Start.

Device#1 LFE5UM-85F: Failed to verify the ID

(Expected: 0x01113043 Read: 0xFFFFFFFF).

 

ERROR - Check configuration setup: Unsuccessful.

 

ERROR - Programming failed.

Please let me know.
Best regards.