This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101: OPT3101:SDK Calibration problems

Part Number: OPT3101

Hi Alex,

As discussed in the other thread: https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1100949/opt3101-sdk-calibration-problems/4091915#4091915

I have added metal shield to my design. I have completed all the calibrations.

After calibration, my internal crosstalk is 3.4 and illumination crosstalk is 74.4. I am loading my crosstalk values in flash location.

But i am still getting wrong distance readings.

With my target set to a fixed distance, the results i am getting are varying amplitude and varying distance with fixed target.

Also, the distance value doesn't make any sense. Can you help me with this?

Regards

Heena

  • Hi Heena,

    How does the metal shield connect to your PCB?

    Best,

    Alex

  • Hi Alex,

    Thank you for all you help so far.

    I have managed to generate relevant distance readings.

    I just have a last question. The distance readings I am getting are little different from actual reading.

    At an actual distance of 300mm, I am getting 100 mm or so.

    What could be the reason for that?

    Regards

    Heena

  • Hi Heena,

    Good to hear you are able to make progress. Distance accuracy at first order will depend on your phase offset calibration, especially if it is a constant offset.

    After that, all the calibrations could impact as well (over temp, crosstalk, etc). 

    Best,

    Alex

  • Hi Alex,

    Thank you for your help.

    I have one more question. I noticed that when my light covers two different distance, the output distance is an average of those two distances.

    Is there anyway I can resolve this averaging problem?

    Regards

    Heena

  • Hi Heena,

    This is a fundamental property of these type of systems. You would need to use a narrower field of view emitter to decrease the detection area or increase the reflectivity of your target relative to the surroundings. The "averaging" acts like a weighted sum by the intensity of reflected light.

    Best,

    Alex