Hello Team,
I'm posting on behalf of my customers.
1) I have used the current vitalab matlab code provided by TI team to get data on the readings for small size object of less than 5mm at a controlled distance of 20cm using the IWR1443Boost sensor SDK version of 2.1
I would like to ask the following:
1) What are some tweaks that can be done to the vitalab matlab code / C code to detect the small size object of less than 5mm ?
2) Is there other projects provided by TI team that could be loaded into the IWR1443Boost to detect small size object of less than 5mm?
3) is there any detailed calibration instruction to configure the IWR1443Boost radar sensor such that the radar is able to detect small object size of less than 5mm ?
4) If IWR1443Boost radar sensor is unable to detect small object of less than 5mm , what are the alternative sensor available from TI that is specific to detect small object size of less than 5mm?
Regards,
Renan