Other Parts Discussed in Thread: AWR1843AOP
Hi,
I am interested in running the labs\lab0011_mrr_beamsteering demo on AWR1843AOP as mentioned in the below thread
I going through this thread And you mentioned there is no changes required for running labs\lab0011_mrr_beamsteering on AWR1843AOP.
and,
1) I want change the no of beams out of 7 beams to 2 beams, so the below function gMrrMSSMCB.steer_Angle value will update/ changes is enough or is it required any other changes.
gMrrMSSMCB.subframeId = 0;
Get_PhaseTxShifterCodeValue(gMrrMSSMCB.steer_Angle, &tx1phcode, &tx2phcode, &tx3phcode);
Cfg_TxPhaseShiftInitParams(&g_ptrtxPhaseShiftCfg, tx1phcode, tx2phcode, tx3phcode );
Semaphore_post (gMrrMSSMCB.phShftSemHandle);
gMrrMSSMCB.steer_Angle = gMrrMSSMCB.steer_Angle + 20;
if(gMrrMSSMCB.steer_Angle >= 60)
{
gMrrMSSMCB.steer_Angle = -60;
}
2) If I want change beam size from 20 degrees to 7 degrees where can I do these modifications/ updates?
Thanks in advance.
Regards
Ravikumar.