This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: Want to use People counting example code directly on

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: IWR1843, IWR6843

Hi Team,

I am working on IWR1843BOOST board. I want to use people counting example on IWR1843BOOST however the binaries present in this location (C:\ti\mmwave_industrial_toolbox_4_12_0\labs\People_Counting\3D_People_Counting\src\68xx) are only related to 68xx .

 I also checked the migration document however there is no direct reference for migrating code from xWR_68xx to IWR1843 . It is via 1642. 

In one of the forum Q/A related to same topic it was mentioned that the binaries from 1642 can be directly used on IWR1843Boost. However it was part of "mmwave_industrial_toolbox_4_1_0" older version of toolbox. Can you please point me to right source code or binaries to be used for people counting example that can be run on IWR1843BOOST EV board. 

Request to please let me know if you need any further details. 

Regards,