Dear TI experts,
I am designing an FDC2214 capacitance measurement system with active shielding.
I have some questions about the ground plane settings.
1. The FDC2214EVM has a portion of the ground plane on the power plane (mid-layer 2).
In my design, the power plane is also smaller than the ground plane size.
So, is there any special use for this ground plane, or does it necessary?
power plane of FDC2214EVM
front and ground plane
bottom and power plane
2. My sensing front ends are coplanar parallel plate electrodes, one connected to CHxA and the other connected to the ground plane of PCB.
Will the electric field excited by the sensor in this way be stably emitted from the CHxA electrode to the ground electrode?
And is there a limit to the trace width?
3. The layout guidelines in the datasheet state that all channels need matched trace lengths, but since I've added buffers, the trace lengths are slightly different for each channel, will this make a big difference to the measurement accuracy?
Best regards,
Will