This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM75A: Conversion time and SCL freq

Part Number: LM75A

Hi,

In LM75A datasheet, t conversion time is mentioned as 100ms to 300ms with a note that specifies that LM75A should not be accessed continuously with a wait time of less than 300ms. As if it happens, the conversion that in progress will be interrupted.

Although during implementation, the access time interval is ~10ms.

Do you see a problem in that.

Regards,

Sunney