Hello ,
I have a problem with our custom design board.Actually I have a lot of problems with our boards but cant figure out the reasons.
One of them is like this :
I succesfully load the debug bin file to the board.But when I try to debug MSS is stucked at soc_init.
I assemled 8 cards but only 2 of them is working now.I can use this two board and I dont get errors.But other boards have problems so I control all the voltage level and sop voltage level for bin file loading and debugging.All voltage levels are same with the working one.Because of that I coudnt find the main reason of this errors.
But I will go one step further if you help me with the above problem.
Thanks
EMRE